+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
The Electroscope is a simple device used to detect the presence of electrostatic charge and to observe phenomena related to static electricity. Its operation is based on the principle of mutual repulsion of unidimensional charges, allowing the presence and relative magnitude of electrification of a given body to be visualised. Electroscopes are mainly used for teaching and experimental purposes, especially in teaching the basics of electrostatics.
The classic design of an electroscope comprises a metal rod terminated by a plate or ball, to which two thin metal leaves (usually gold or aluminium) are attached, housed inside an air-protective shield. In the uncharged state, the strips adhere to each other, but when a charge is applied, they diverge under the forces of electrostatic repulsion. The angle at which the leaves diverge depends on the amount of charge accumulated, although the electroscope does not allow an exact measurement of the charge, but only a qualitative assessment.
There are also versions of electroscopes with a needle that rotates due to a potential difference, allowing more precise observations. Modern versions sometimes use electronic components to detect and amplify electrostatic effects, but the principle of operation remains unchanged.
Electroscopes show sensitivity to environmental influences, including air humidity, which can affect the discharge of accumulated charges. For this reason, the instrument functions best under dry laboratory conditions. In the past, electroscopes were also important in the study of ionising radiation, as detectors to detect ionisation of the air causing gradual leaf fall, before being replaced by more precise measuring instruments.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.