+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Idempotence - definition

Idempotency is a mathematical and computer science concept describing the property of an operation whose repeated application produces the same result as performing it once. Formally, for a binary operation f, operating on a set X, the function is idempotent if, for each element x in the set, the equality holds: f(x, x) = f(x). In the context of unary functions, this condition simplifies to the form f(f(x)) = f(x), which means that applying the function to its own result does not change the result.

In computer science, idempotency plays a fundamental role in the design of distributed systems, network protocols, databases and web services. For example, an HTTP PUT request is idempotent because repeatedly sending the same operation to the server does not change the state of the resource beyond the first execution - thus providing repeat resistance in the event of a network failure.

In algebraic abstract structures such as semigroups, monoids or Boolean algebras, idempotency serves as a classification criterion for logical operations (e.g. conjunction, alternative) and projective functions. In functional programming and mathematical logic, the concept also refers to constructions that ensure deterministic and predictable operation without side effects. In engineering practice, idempotency promotes the design of fault-tolerant, easily testable and reconfigurable systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO