+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

IGBT - definition

The IGBT (Insulated Gate Bipolar Transistor) is a semiconductor power element that combines in its structure the characteristics of a bipolar transistor (BJT) and an insulated gate transistor (MOSFET). It is designed to provide high switching efficiency while maintaining high current-carrying capability. With this combination, the IGBT is widely used in power electronics systems where low conduction losses and fast switching response are crucial.

The IGBT has a voltage-controlled input - as in a MOSFET transistor - which simplifies its control circuitry and reduces gate power consumption. At the same time, in the conducting state, the bipolar structure allows significant currents to be carried at a relatively low saturation voltage, resulting in high power efficiency. A characteristic feature of this element is the presence of a p-type layer in the power structure, which allows more efficient conduction of current in the on-state.

In practical applications, IGBTs are used in inverters, converters, UPSs, motor control systems, HVDC systems and various types of industrial equipment. Their ability to operate at high voltages and currents makes them the preferred solution for medium- and high-voltage power applications. The performance of an IGBT, such as switching time, power loss or resistance to overload phenomena, depends on its design and operating conditions, including cooling and supply voltage.

Due to its complex structure, IGBTs exhibit delayed current turn-off phenomena associated with carrier charge recombination in the bipolar part, which affects dynamic characteristics. Nevertheless, thanks to the continuous development of technology, today's IGBT transistors achieve very high efficiency and reliability, enabling their use in increasingly demanding power conversion and control systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO