+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Inclinometer - definition

An Inclinometer is a measuring instrument used to determine the angle of inclination of an object with respect to a selected reference level, usually in relation to the horizontal plane. Depending on their design, inclinometers can measure one-dimensional or two-dimensional tilt, providing information on the deviation in one or two perpendicular axes. They are used in civil engineering, geotechnics, mechanics, robotics, Industrial Robotics, and navigation systems.

The operation of an inclinometer is based on the detection of a change in position relative to a gravitational force vector. In analogue devices, this is realised through mechanical components such as pendulums, bubbles in a liquid or moving masses. Modern designs use MEMS (micro-electromechanical) sensors, which measure gravitational accelerations and convert them into tilt angles. These devices offer high precision and can be integrated into electronic systems, enabling digital readout and data transmission.

Inclinometers are particularly useful in monitoring the stability of engineering structures such as dams, bridges, buildings or embankments, where even small deviations can indicate deformations or structural risk. In geotechnics, they are used to measure displacements in soils or slopes by placing probes in special measuring holes. In robotics and mobile electronics, they act as orientation sensors, enabling platform stabilisation and path correction.

The measurement accuracy of an inclinometer depends on its design, measurement range, resistance to interference and quality of calibration. In many applications, resistance to vibration, temperature fluctuations and other environmental factors is also important. In combination with other sensors, such as gyros or magnetometers, inclinometers are part of complex inertial navigation and technical diagnostic systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO