+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Intermodulation - definition

Intermodulation is a non-linear phenomenon involving the formation of additional signals at new frequencies as a result of the simultaneous interaction of two or more waves of different frequencies in a non-linear electronic circuit. These frequencies are combinations of sums and differences of integer multiples of the input signals and are not present in the original signal, which can lead to distortion and interference in the transmission path.

The phenomenon of intermodulation occurs primarily in radio equipment, amplifiers, frequency mixers, filters and other components that do not behave fully linearly to the signals. In practice, lower order (e.g. third order) intermodulation products are particularly important, as they can occur close to the useful band and interfere with transmission. In wireless communication systems, intermodulation can lead to signal overlap, reduced transmission quality and degradation of the signal-to-noise ratio.

In radio engineering and telecommunications, the level of intermodulation is analysed as one of the key quality parameters for transceivers. This uses, among other things, the intermodulation factor (IP - Intermodulation Product) and the third-order crossover point (IP3), which determine the system's ability to operate with multiple signals without generating excessive distortion. Measuring and reducing intermodulation effects are essential in the design of multi-channel systems such as base stations, SDR receivers, measurement equipment or high-end audio systems.

This phenomenon is universal and can also occur in acoustics and in light technology if signals interact with elements with non-linear properties. In electronics, its presence is most often indicative of imperfect components or component overload, so one of the goals of circuit design is to minimise the effects of intermodulation in the usable range.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO