+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Kinematics - definition

Kinematics is the branch of classical mechanics concerned with describing the motion of bodies without regard to the forces causing it. Its aim is to mathematically represent the relationship between displacement, velocity, acceleration and time for objects moving in one-, two- or three-dimensional space. Others types of motion - progressive, rotational and complex - are analysed in kinematics using the tools of differential calculus, geometry and reference system theory.

The basic concept in kinematics is the trajectory, which defines the geometry of the path a point or material body takes. From it, kinematic quantities such as instantaneous velocity - which is the derivative of position with respect to time - and acceleration, which is the derivative of velocity, are determined. In the case of rotational motion, the analogous quantities are angular velocity and angular acceleration. Kinematics also uses different coordinate systems, such as Cartesian, polar or cylindrical, depending on the nature of the motion being analysed.

In engineering, kinematics plays a key role in the analysis and design of mechanisms, robots, manipulators or drive systems. It allows the precise modelling of the trajectories of movement of machine components without the need to take dynamic interactions into account. Mechatronics and robotics use both direct kinematics, which is used to determine the position of an effector based on known input parameters, and inverse kinematics, in which the aim is to determine the required control values to reach a given position.

Kinematics is also used in computer animation, biomechanics, aerodynamics and motion analysis in sports and medicine. In research, it provides a starting point for further dynamic analyses that take into account forces, moments and mass properties of moving objects. Its descriptions are the basis for the formulation of equations of motion within other branches of mechanics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO