+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Cogeneration - definition

Cogeneration, also referred to as combined heat and power (CHP), is a technology for the simultaneous generation of electricity and heat in a single process, usually in combined heat and power plants or decentralised generation units. Unlike traditional methods of energy production, in which a significant proportion of primary energy (e.g. fuels burned) is lost as waste heat, cogeneration enables it to be managed efficiently, significantly increasing the overall efficiency of fuel chemical energy conversion.

A typical CHP system consists of a reciprocating engine, a gas or steam turbine, coupled to an electric generator, and a heat exchanger that recovers heat energy from exhaust gas, coolant or process steam. The recovered heat can be used for heating buildings, industrial processes, hot water production or absorption cooling systems (trigeneration).

From an energy engineering perspective, cogeneration makes it possible to increase the overall energy efficiency from a typical 35-40% in a conventional power plant to as much as 85-90% in well-designed cogeneration systems. CHP technologies can run on both fossil fuels (natural gas, fuel oil) and renewable fuels (biogas, biomass), making them an important tool for energy transformation.

CHP plays a strategic role in the district heating sector, especially in countries with cold climates and high demand for useful heat, and its development is supported by climate policies and market mechanisms that promote energy efficiency and reduce greenhouse gas emissions. It does, however, require adequate balancing of heat and electricity demand and a transmission infrastructure suited to real-time dynamic management of energy flows.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO