+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Swedish Wheel is a specialised type of mechanical wheel that allows a vehicle or mobile platform to move in multiple directions without changing the orientation of the entire running gear. Its design is based on a main supporting wheel with transversely oriented, independently rotating rollers around its perimeter. This makes it possible to generate movement along the wheel's main axis, as well as in the transverse direction, thus realising holonomic movement - fully free in two plane dimensions.
Swedish Wheels are primarily used in mobile robotics, Industrial Robotics and material handling systems where high precision manoeuvring in confined spaces is required. Their unique geometry allows them to move smoothly in any direction, rotate about their own axis and move along complex trajectories without the need for traditional turning. Actuators are often used in omniwheel class robots and platform vehicles with independent drive for each wheel.
In mechanical practice, the design of a Swedish wheel requires a precise arrangement of the rollers and ensuring their free rotation, which involves the use of suitable Bearings and low-friction materials . The correct choice of the number and shape of the rollers has a direct impact on the smoothness of movement and the ability to carry loads. Due to the complex dynamic characteristics, the control of Swedish Wheels vehicles requires advanced kinematic modelling and precise synchronisation Actuators.
In engineering applications, the Swedish Wheel is an example of a mechatronic solution in which mechanics, electronics and control algorithms work together to achieve high manoeuvrability and flexible motion. Hybrid variants are also being developed, combining the features of Swedish Wheels and traditional running gears to enable adaptation to different terrain conditions and operational scenarios.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.