+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Electrochemical corrosion is the process of deterioration of a material, usually a metal, as a result of electrochemical reactions occurring on its surface in the presence of an electrolyte. This phenomenon involves the flow of electrons between areas of metal at different electrochemical potentials, leading to the oxidation of the metal at the anode site and its gradual degradation. At the same time, reduction reactions take place at the cathode site, usually involving oxygen or hydrogen ions contained in the electrolytic solution.
The mechanism of electrochemical corrosion is based on the formation of local galvanic cells, in which potential differences may result from material inhomogeneities, the presence of different metallic phases, mechanical stresses or varying environmental conditions. In such cells, the metal passes into solution in the form of ions, resulting in weight loss, deterioration of mechanical properties and changes in surface structure. This process can occur uniformly over the entire surface or locally, leading to pitting, cracking and perforation.
Electrochemical corrosion plays an important role in materials engineering, electrical engineering and industrial construction, where it affects the durability and safety of installations, equipment and metal components. It is particularly dangerous in humid, marine environments or those exposed to aggressive chemicals such as chlorides or acids. This phenomenon also occurs in electronic circuits, where moisture and contamination can lead to the degradation of solder joints and conductive pathways.
Managing electrochemical corrosion involves the use of protective coatings, corrosion inhibitors, electrolyte-resistant materials and electrochemical techniques such as cathodic protection. Understanding the mechanisms and factors influencing the development of corrosion is critical to the design of durable and reliable engineered systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.