+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
LORAN (Long Range Navigation) is a long-range radio navigation system based on the measurement of the difference in reception times of radio signals emitted by a network of terrestrial transmitters. It works on the principle of hyperbolic localisation, making it possible to determine the geographical position of a ship, aircraft or other object moving in space by analysing the propagation times of radio waves between a receiver and a pair of transmitting stations.
The LORAN system uses low-frequency (LF) radio waves, which, thanks to their propagation properties, allow the signal to be transmitted over very long distances, often exceeding thousands of kilometres. Each set of transmitters consists of one main station and a number of secondary stations that send synchronised radio pulses at precisely defined time intervals. The receiver compares the moments of arrival of the signals from the different stations and, on this basis, determines a hyperbola of possible locations, and the intersection of several such hyperbolae makes it possible to determine the exact position.
The system was developed during the Second World War in the United States and played an important role in maritime and aeronautical navigation for several Decades. Due to its ability to operate in harsh atmospheric conditions and its independence from satellites, LORAN was considered a stable and fault-tolerant tool to aid spatial orientation, especially in polar and oceanic regions.
The modern version of the system is eLORAN (enhanced LORAN), which offers greater accuracy, synchronisation with atomic time and integration with modern navigation systems, including GPS. With its enhanced immunity to electromagnetic interference and ability to operate under satellite signal interference, eLORAN is being considered as an alternative or backup system to global satellite navigation systems in the context of critical infrastructure security.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.