+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Radio waves are a type of electromagnetic waves with the lowest frequencies and the longest wavelengths in the entire electromagnetic spectrum, ranging from several hertz (Hz) to several hundred gigahertz (GHz). They are generated by the accelerated motion of electric charges and propagate through space as varying electric fields and magnetic fields, oscillating perpendicular to each other and to the direction of propagation.
The properties of radio waves, such as their ability to travel long distances, penetrate the Earth's atmosphere, and reflect off the ionosphere, make them useful for transmitting information in telecommunications, navigation, radar, and data transmission systems. These waves can propagate in various modes: along the Earth's surface (surface waves), through reflections from atmospheric layers (ionospheric waves), or in a straight line through space (space waves).
Due to the wide range of frequencies, radio waves are divided into bands, among which long, medium, short, and very short waves are distinguished, each with different propagation properties and applications. The characteristics of radio wave propagation depend strictly on frequency, atmospheric conditions, propagation environment properties, and effects such as diffraction, refraction, and attenuation.
In communication technology, radio waves form the basis of systems such as radio broadcasting, terrestrial television, mobile telephony, satellite communication, Wi-Fi, and various industrial and military applications, including radars and radio frequency identification systems RFID. In signal transmission, radio waves can be modulated in terms of amplitude, frequency, or phase, allowing for the transmission of data in analog or digital form.
Radio waves are generated in specially designed transmitting circuits, using high-frequency oscillators, power amplifiers, and antennas emitting waves in a specific direction or omnidirectionally. Reception of waves is carried out using antennas and detection and demodulation systems, which enable the recovery of transmitted information. In the context of advanced scientific research, radio waves are also used in radio astronomy, for observing natural sources of electromagnetic radiation in space, such as pulsars, galaxies, and nebulae.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.