+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Herc (Hz) is the unit of frequency measurement in UoM, denoting the number of times a given cyclic phenomenon repeats in one second. It is named after the German physicist Heinrich Hertz, who was the first to experimentally confirm the existence of electromagnetic waves predicted theoretically by Maxwell. One hertz means one cycle per second (1 Hz = 1/s), and the unit is used in all fields of science and technology related to periodic motion, vibrations and waves.
In electrical engineering and electronics, the hertz is used to describe the frequency of alternating voltages, digital signals, resonant vibrations or the timing of microprocessor systems. For example, the power grid in Europe operates at 50 Hz, which means that the voltage changes its polarity 50 times per second. In computer systems, the clock frequency of a processor is expressed in megahertz (MHz) or gigahertz (GHz), indicating the number of operations that can be performed per unit time.
In acoustics hertz determines the pitch of sound, which is the frequency of vibration of air molecules perceived by the human ear. In communications and radio engineering, determines the position of transmission channels in the electromagnetic spectrum, with multiples of the hertz unit often used, such as kilohertz (kHz), megahertz (MHz) or gigahertz (GHz), corresponding to thousands, millions or billions of cycles per second respectively.
Frequency is a fundamental quantity in signal analysis, filter design, modulation systems, vibration measurement and in any field where time-varying processes occur. The Hertz as a unit facilitates the unambiguous expression and comparison of these phenomena on a time scale.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.