+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Attenuation is the physical phenomenon of a gradual reduction in the amplitude of a vibration, wave or signal as it propagates through time or space. This process is due to the presence of energy losses, which can be mechanical, electrical, thermal or material - depending on the type of system and the transmission environment. In technical terms, attenuation describes the efficiency of energy extinction and is one of the key parameters in the analysis of dynamic, acoustic, electronic and optical systems.
In electrical engineering and telecommunications, attenuation refers to the loss of signal power during transmission through a transmission line, cable, waveguide, optical fibre or any Passives element. It is usually expressed in decibels (dB) as the ratio of input power to output power, and depends on the frequency, the length of the transmission path and the characteristics of the medium. Attenuation has a significant impact on signal quality, transmission range and the need for amplifiers or signal regeneration in digital systems.
In mechanics and acoustics, damping describes the ability of a system to dissipate vibrational energy through friction, viscous drag, losses in elastic materials or conversion of mechanical energy into heat. In resonant systems, the damping coefficient determines the rate of disappearance of free oscillations and determines the resonant bandwidth. It is of key importance in the design of damping systems, measurement systems, mechanical structures and acoustic enclosures.
Damping can also be a deliberately introduced system property - e.g. in attenuators, filters or matching circuits - to reduce noise, prevent overdrive, protect equipment or shape the frequency response. In engineering applications, modelling and control of damping is important, both in the context of stability analysis and system performance optimisation.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.