+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

MMIC (Monolithic Microwave Integrated Circuit) - definition

MMIC (Monolithic Microwave Integrated Circuit) is a monolithic integrated circuit operating in the microwave frequency range, typically from a few MHz to hundreds of GHz. Unlike traditional electronic circuits, an MMIC integrates all active and passive components - such as Transistors, Resistors, Capacitors or transmission lines - into a single semiconductor structure, typically made of Gallium Arsenide (GaAs), Gallium Nitride (GaN) or Indium Phosphide (InP). These semiconductor materials exhibit better high-frequency properties than silicon, making them more effective in microwave applications.

MMIC technology is used in satellite communication systems, radars, RF transmitters and receivers, military equipment and wireless telecommunications. Thanks to its compact design, high reliability and repeatable performance, MMICs enable miniature and efficient RF circuits with a very wide bandwidth.

The MMIC design and fabrication process is similar to microelectronic technologies, but requires specialised simulation tools and precise control of geometrical parameters and material properties. Optimising impedance matching and minimising propagation losses in the millimetre-wave range are crucial. Due to high-frequency operation, designers must take into account phenomena such as electromagnetic coupling, phase delays or parasitic effects.

The MMIC is an essential component of modern RF and microwave systems, especially where high integration density, temperature stability and high output power are required while miniaturising the circuit.

Integrated circuits MMICs

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO