+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Voltage booster converter (boost converter) - definition

A Boost Converter (boost Converter) is a type of power electronic DC-DC converter designed to increase the DC voltage from the input level to a higher voltage at the output. This type of circuit is widely used in power electronics, battery systems, the automotive industry and also in renewable energy, particularly in photovoltaic applications.

The principle of the boost converter is based on the cyclic storage of energy in the magnetic field of an inductive coil during the conduction of a switching element (usually a transistor) and its transfer to the load when the transistor is switched off. During the off phase, the energy stored in the coil attaches to the source voltage, causing the voltages to add up and produce a higher level at the output. Control is usually by pulse width modulation (PWM), which allows the output voltage to be precisely regulated.

A characteristic feature of a boost converter is that the output voltage is always higher than the input voltage, but in practice this relationship is limited by the power efficiency internal resistances and the operating range of the power components. In typical applications, voltage ripple filtering, overcurrent protection and dynamic parameter control are also taken into account to ensure stable operation.

In advanced designs, boost converters can be integrated with other DC-DC circuit topologies to achieve a wider voltage regulation range, higher efficiency or protection functions. The design of such systems requires consideration of many factors, including the nature of the load, electromagnetic interference and thermal requirements.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO