+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
A block diagram is a graphical representation of the functional structure of a technical, logical or process system in which the individual components and operations are represented as blocks connected by signal lines or information flow relationships. It is used to illustrate the general principle of operation of systems or algorithms, without going into implementation details of individual components. It is used extensively in engineering, computer science, Automation, electronics and the organisation of industrial and information processes.
In a block diagram, each block is responsible for a specific function or module, such as signal processing, control, data transmission, information storage or the execution of logical or mathematical operations. Lines connecting the blocks indicate the direction of data, energy or control flow. The use of standard symbols and conventions - depending on the field - enables the diagram to be read unambiguously by specialists in different technical fields.
Block diagrams are used at the design, analysis, documentation and engineering communication stages. They facilitate the understanding of complex systems and support modelling, optimisation and diagnostic processes. In Automation and Control systems, they are used to represent the structure of regulation, the relationship between measurement and control signals, and the configuration of PID or feedback systems. In programming, on the other hand, they are used to describe the logic of algorithms and data flow in computer programmes.
The advantages of the block diagram are its readability, modularity and the possibility of rapid modification and adaptation to different versions of the design. In combination with other forms of technical documentation, it is an indispensable part of the engineering process, enabling a systematic approach to the design and analysis of complex systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.