+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

VRM (Voltage Regulator Module) - definition

VRM (Voltage Regulator Module) is a modular electronic circuit responsible for stabilising and delivering a precisely specified supply voltage to components requiring precisely controlled power levels, such as processors, GPUs, memories or other advanced digital circuits. The VRM has a key function in modern computer systems and electronic devices where the input voltage varies significantly with the requirements of the consumers.

Technically, the VRM is typically a buck pulse converter (voltage step-down) that dynamically adjusts the output voltage level in response to varying load and operating conditions. It consists of a controller PWM (Pulse Width Modulation), power transistors (usually MOSFETs), inductor, filter capacitors and measurement circuits. VRM operation is based on cycling the power transistors on and off to regulate the average voltage at the output, while minimising energy loss.

Today's VRMs used in computer and server motherboards must meet stringent requirements for voltage stability, speed of response to load changes and energy efficiency. This is particularly important when powering central processing units (CPUs) and graphics processing units (GPUs), which can dynamically vary power consumption depending on the load. Advanced VRM solutions also implement monitoring, thermal and current protection functions and support for voltage regulation according to CPU manufacturers' specifications (e.g. Intel VRD, AMD SVI).

The performance of the VRM has a direct impact on the system's stability, its overclocking capabilities and the overall power culture of the device. Both electronic and thermal aspects are crucial in the design of VRMs, making them one of the most advanced power components in today's computing platforms.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO