+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Date of publication: 27-06-2023 🕒 2 min read
BM Group is a leading Italian manufacturer of fasteners and solutions from the field of electrical systems. The company is focused on manufacturing cable terminals and lugs, cabling accessories and equipment as well as crimping tools for connectors and terminals.
Automatic crimping pliers with replaceable dies help prevent damage of the cables (individual strands of the conductor), as well as connectors and ferrules. They are characterised by a wide crimping range and are ready to work with cables whose diameter ranges from 0.25 mm2 to 16 mm2. They also boast compatibility with various types of terminals and connectors. Replaceable dies ensure optimal contact crimping quality, which helps minimise its electrical resistance and guarantees safe operation of electric devices. The crimping tool adjusts automatically to the size of connectors and end sleeves/ferrules. Because the pliers may only be opened after they have been fully closed, you can always be sure that the element is crimped with the right force.
The crimping tool described here is delivered with a set of dies. The entire kit is composed of:
Keep in mind that the TME catalogue includes other crimping tool kits with connectors and end sleeves by the BM Group. Just like in the case of BM5345, the manufacturer supplies them together with special transport cases which make work in the field easier and faster.