+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

H-infinity - definition

H-infinity (denoted H∞) is a mathematical and engineering concept used in control theory, signals and systems theory, referring to a class of norms and methods for designing fault-tolerant systems. In the context of linear systems analysis, H∞ defines the norm of a system's transfer function as the maximum gain of the input signal relative to the output signal in the frequency domain. Formally, the H∞ norm is equal to the supremum of the largest value of the singular transmittance along the complex axis.

This concept is used in the design of resilient control systems (robust control), where the aim is to ensure stability and performance despite uncertainties in model parameters, disturbances or non-linearities. Unlike classical methods based on the minimisation of the mean-square error, the H∞ approach focuses on the worst-case scenario - the maximum disturbance energy the system can pass through - making it a more conservative but also safer tool for critical applications.

From a systems theory point of view, the H∞ space contains all stable and proper norm-limited complex functions defined on a positive-frequency complex half-plane (for continuous systems) or inside the unit Wheels (for discrete systems). Analysis and synthesis in this space is based on Tools such as linear matrix inequalities (LMIs), Riccati transformations and the Bounded Real Lemma theorem.

The H∞ standard and associated design algorithms are widely used in advanced engineering fields such as flight control, adaptive systems, mechatronics or high-precision electronics, where it is crucial to maintain high quality control regardless of varying operating conditions and disturbance patterns.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO