+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Negative feedback is a control mechanism that reverses part of the system's output signal to its input in such a way as to counteract the original control signal. In practice, this means that the feedback signal is subtracted from the input signal, leading to a stabilisation of the system's performance and reducing the influence of noise, non-linearities and changes in component parameters.
In electronics, negative feedback is used primarily in amplifier systems, Regulators and Automation systems. It allows precise shaping of the frequency response, limiting non-linear distortion and controlling gain. It allows the system to achieve greater linearity and better dynamic response, as errors between the input and output signals are automatically corrected by a self-adjusting mechanism.
This phenomenon has a basis in both circuit theory and control theory, where it is regarded as a Tools for improving the accuracy and reliability of system performance. In the context of analogue systems, a typical example of the use of negative feedback is an operational amplifier operating in an inverting or non-inverting configuration, where the feedback determines the gain and range of linear operation. In digital or mixed systems, it can occur as part of a control loop, e.g. in voltage converters or motor control systems.
A characteristic feature of negative coupling is its ability to increase the stability of the system, although at the same time it can lead to a reduction in overall gain. The balance between these properties is crucial in the design of systems that need to operate efficiently under varying environmental conditions and loads.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.