+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Faraday cage - definition

A Faraday Cage is a conductive structure designed to shield the internal space from external electrostatic and electromagnetic fields. The principle of operation is based on the phenomenon of charge distribution on the surface of the conductor - in response to an external electric field, the charges in the conductive shield move in such a way that a field of the opposite direction is generated inside the structure, effectively cancelling the influence of the external field. As a result, the inside of the cage remains shielded, meaning that external signals do not affect the equipment or people inside.

A Faraday cage can take many forms, from solid metal shields to conductive mesh structures, which, despite the openings, effectively attenuate electromagnetic waves with wavelengths greater than the size of the slots. Its effectiveness depends on the type and thickness of the material, the accuracy of the conductive connections and the frequency of the waves to be attenuated. In practice, this phenomenon is used in the construction of shielded test rooms, electronic equipment enclosures, signal cable shielding or electromagnetic emission protection (EMC) systems.

In industrial and laboratory applications, Faraday cages protect sensitive equipment from radio interference, electromagnetic pulses (e.g. ESD, EMP) and lightning discharges. At the same time, they prevent the emission of interference generated inside the device, which is crucial in the context of electromagnetic compatibility (EMC) and meeting compatibility standards with other systems. In data protection, they are also used in the form of Guards for electronic equipment to prevent unauthorised wireless communication.

The term Faraday cage is derived from Michael Faraday, who in the 19th century was the first to describe the phenomenon of electrostatic shielding and its applications in experimental practice.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO