+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Date of publication: 30-05-2025 🕒 4 min read
In the world of electronics and classical physics, electromagnetic phenomena play a crucial role. To understand how electric motors, generators, transformers, or inductive sensors work, we can use auxiliary tools. In this article, you will learn about the right-hand rule and the left-hand rule, which help intuitively visualize the directions of force actions and current flows in magnetic fields.
The right and left-hand rules, when we learn them in school, seem merely mnemonic techniques to facilitate remembering elementary issues. Meanwhile, they are fundamental tools for anyone who wants to understand how the world of electromagnetism works. They are crucial in the analysis and design of electronic systems, motors, generators, or sensors. Mastering these rules is the first step to becoming a conscious creator of technology.
The right-hand rule is mainly used in the context of electromagnetic induction. We use it to determine the direction of the electromotive force (EMF) and the induced current in a conductor moving in a magnetic field. The direction of the EMF corresponds to how the current would "try" to flow in an open or closed circuit. The EMF is always "oriented" to counteract the cause that induced it (according to Lenz's Law, which will be discussed later).
How to apply?
Application of the Right-Hand Rule:
B – Magnetic induction vector (magnetic field)
v – Speed of conductor or particle movement
F – Force
The left-hand rule helps determine the direction of the electrodynamic force (Lorentz) acting on a conductor with current in a magnetic field. It is fundamental to the operation of electric motors.
How to apply?
Application of the Left-Hand Rule:
The electromagnetic field is a combination of an electric field and a magnetic field, which together create a dynamic structure affecting electric charges and conductors with current. The direction of the electric field is defined as directed from the positive charge towards the negative charge. Imagining a single positive charge, the field radiates outward from it, while for a negative charge, the field lines direct inward.
The magnetic field has a direction determined by the course of magnetic poles – in the external space of the magnet, it runs from the north pole (N) to the south pole (S). Inside the magnet, however, the field lines close, flowing from the south pole to the north, forming closed loops.
The hand rules also help understand the behavior of charges moving in a magnetic field. The Lorentz force acts on a charged particle moving with a certain speed in a magnetic field – this is crucial in:
For positive particles, the left-hand rule is used, for negative ones – the direction of the force is opposite.
Lenz's Law can be understood as a practical application of the right-hand rule and the principle of energy conservation: The induced current always opposes the cause that induced it.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.