+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Date of publication: 02-06-2025 Update date: 24-03-2026 🕒 7 min read
Robots are entering more and more aspects of our lives, becoming an integral part of both industry and home environments. From automated production lines, where robots perform repetitive and precise tasks, to intelligent vacuum cleaners that autonomously maintain the cleanliness of our floors, robot programming plays a crucial role in their efficient operation. In this article, we will answer key questions about robot programming: What methods and tools are used to program industrial and domestic robots? What programming languages dominate these two areas and what are their specific applications? What should be paid special attention to when starting out with robot programming in order to effectively utilize their potential?
Robotics is a field that is dynamically developing, affecting various aspects of our lives. Thanks to technological progress, robots not only increase production efficiency but also improve the comfort of everyday life.
Industrial robots have revolutionized many industries, taking over tasks that require repeatability, precision, or are dangerous for humans. Their versatile applications include:
Many companies opt for offline robot programming to avoid costly production downtime. Control programs for robots are created and tested in a virtual environment, then transferred to the robot. Popular tools for offline programming and simulation include:
Industrial robots require specialized programming languages and environments that provide precise control and synchronization with other devices:
In addition to traditional programming languages, graphical programming tools are gaining popularity, simplifying the process of creating programs for robots. An example of such a tool is VAL BLOCKS from Stäubli, which allows robot programming using an intuitive "drag and drop" interface. This enables even those without advanced programming knowledge to create simple applications for robots.
Domestic robots are gaining importance, offering support in daily activities, entertainment, and education. It is worth noting that their role goes beyond toys – they become real assistants in many aspects of home life. Examples of domestic robot applications:
Many domestic robots, especially educational ones, offer programming capabilities, allowing customization of their behavior and interactions. Programmable educational robots that help in learning coding include:
More advanced models of domestic robots offer extensive customization options:Setting work schedules: automating daily tasks such as cleaning saves time and increases the comfort of life. Defining cleaning zones: users can specify which areas of the home should be cleaned and which should be omitted, which is particularly useful in homes with different types of floors or obstacles. Uploading software updates: regular updates add new features, improve performance, and enhance robot security.
The tools and programming languages in robotics vary depending on the robot's applications. In industrial robotics, a low-level approach dominates, ensuring efficiency and precise control:
Frameworks such as ROS (Robot Operating System) facilitate the creation of complex robotic applications, providing a set of tools and libraries for communication, perception, and motion planning. In domestic and educational robotics, programming is usually simpler and more accessible:
Popular platforms such as Arduino and Raspberry Pi enable the creation of DIY robotic projects, giving users full control over hardware and software.
Check out DIY project suggestions
Robot programming, despite its numerous advantages and benefits, involves a series of challenges that hinder its widespread and effective implementation. Understanding these obstacles is crucial for further development of the field.Complexity of languages and environments: robot programming often requires knowledge of specialized languages (such as KRL or RAPID) and complex programming environments. The variety of available tools and technologies can be overwhelming, and mastering them requires time and effort.Integration with other systems: many companies use existing production or IT systems that may be incompatible with modern robotic solutions. Integrating robots with these systems can be complicated and costly, requiring adjustments to software and hardware.Hardware limitations and real-time operation: robots often need to operate in real time, responding to changing environmental conditions. Hardware limitations, such as computational power or bandwidth, can hinder achieving the required speed and precision of operation.Safety of use: robots, especially industrial ones, can pose a threat to humans if not properly programmed and secured. Ensuring safe collaboration between humans and robots (so-called collaborative work) is a key challenge in robotics.Lack of standardization and difficulty in learning: the lack of uniform standards in robot programming complicates the exchange of knowledge and experiences between programmers. Learning robot programming is often difficult and requires access to specialized training and resources.
However, it is worth noting that starting out in robotics does not always have to involve high costs. There are simulators and educational robot kits available that allow for learning programming and experimenting without the need to invest in expensive equipment.
Programming robots (both industrial and domestic) does not have to be reserved only for specialists. Thanks to available tools and a growing number of educational materials, it is increasingly easy to start your own projects. Numerous practical examples and intuitive programming environments make robotics no longer an abstraction but a real path of development – both at work and in the comfort of home.
For all robotics enthusiasts, both beginners and advanced, TME offers a wide selection of components and tools that will enable the realization of even the most ambitious projects. From microcontrollers and PLC controllers, through sensors and motors, to specialized software and educational kits. We invite you to explore our offer.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.