+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Understanding rolling bearings - structure, operation, and applications

Date of publication: 09-06-2025 🕒 15 min read

Roller Bearings are one of the most widely used mechanical components, that play a key role in reducing friction between moving machine parts. Through the use of moving rolling elements - such as balls, rollers or needle rollers - they enable smooth and energy-efficient rotary motion. Their versatility makes them, their versatility means that they can be found in domestic appliances, as well as in heavy industry and automotive applications.

Although the principle of Bearings is based on a simple idea, their history dates back to antiquity. As far back as Egyptian times, primitive forms of bearings with wooden shafts were used. The modern version of the Roller Bearings was patented in 1794 by Philip Vaughan, a Welsh inventor, who was the first to describe a design with balls rolling in guides between two rings. Bearings have evolved enormously since then, to become an indispensable part of modern technology.

Roller Bearings

How do Roller Bearings work?

The principle of Roller Bearings is based on transforming sliding friction into rolling friction, which translates into significantly lower resistance to motion and higher mechanical efficiency. This makes it possible to efficiently transfer forces and torques with minimal energy consumption.

Friction-reducing mechanism

In Roller Bearings, rolling elements (e.g. balls, rollers, needles) roll between the inner and outer ring, forming a point or linear contact with the raceways. It is this method of contact that significantly reduces the contact area and therefore reduces the resistance to motion.

The movement of the rolling elements takes place on precision-made raceways, which guide them in a defined direction and stabilise the entire structure. The cage also plays a key role: it maintains the correct distance between the rolling elements and prevents them from rubbing against each other.

An additional role is played by appropriate lubrication. The lubricant forms a thin film separating the metal surfaces, which further reduces friction, protects against corrosion and dissipates heat. Depending on the application, either plastic grease or oil is used, and their correct selection has a direct impact on the bearing life and reliability.

How do they differ from plain bearings?

Although both Roller Bearings, bearings and plain bearings have a similar function - making rotary motion possible - they differ in terms of their construction, their operating mechanics and typical applications.

A comparison of the most important features of Plain Bearings and Roller Bearings is shown in the table below:

Feature Roller Bearings Plain Bearings
Type of friction Rolling (balls, rollers) Plain (contact surfaces)
Contact surface Point or linear Full contact surface
Friction Low Higher than Roller Bearings
Wear Low (with correct lubrication) Greater - dependent on materials
Operating speed Suitable for high speeds Better for lower speeds and high loads
Handling and maintenance Requires precision assembly and suitable lubricant Often simple to handle, but require precise fitting
Applications Universal - from household appliances to heavy industry Often used in simple or low-cost mechanisms

Roller Bearings are usually preferred for applications requiring precise motion control, low resistance and high durability. Plain Bearings, on the other hand, are used where simplicity of design is important, where simplicity of design is important, compact size or resistance to large impacts.

Roller Bearings design

To understand the full capabilities of Roller Bearings, it is worth looking at their construction. Although at first glance they are small components, they are made up of many components working together, each of which is important for the proper functioning of the whole mechanism.

Basic components of a Roller Bearing

Every Roller Bearings is made up of several key parts:

  • Inner and outer ring - the inner ring is mounted on the shaft and rotates with it. The outer ring is usually seated in the machine housing and remains stationary. Both rings form raceways, on which the rolling elements roll.
  • the rolling elements are responsible for converting sliding friction into rolling friction. Depending on the type of bearing, these can be balls, rollers, barrels, cones or needles. Their shape influences the bearing characteristics and the type of loads transferred.
  • cage - separates the rolling elements from each other, prevents them from rubbing against each other and ensures even distribution within the raceway. Can be made of metal or plastic, depending on application requirements.
  • Seals and lubricant - many bearings are fitted with seals to protect the inside from dust, moisture and other contaminants. Lubricant (plastic or oil) has a protective role and reduces friction, which has a direct effect on bearing life and trouble-free operation.

Design variants

Depending on technical requirements, bearings can differ both in design, and designations, which you should be able to read.

Bearings designations
Designations such as ZZ, 2RS or C3 provide information on the design features of a particular model:

  • ZZ stands for sheet metal guards on both sides, for protection against dust,
  • 2RS indicates rubber seals on both sides of the Bearings,
  • C3 indicates increased internal clearance (relative to standard clearance), recommended e.g. at higher operating temperatures, at higher speeds or with press fit.

Roller Bearings with radial play C3

Knowledge of these symbols allows the Bearings to be selected for specific environmental and operating conditions.

Open vs. sealed Bearings
Open Bearings have no additional Guards or seals - they are designed for clean environments or centrally lubricated applications. Sealed Bearings (ZZ, 2RS) are ready to operate in harsher environments, where protection from contamination and retention of lubricant within the structure are critical.

Choosing the right design variant has a direct impact on the bearing's durability, reliability and application range of the Bearings.

Classification and types of Roller Bearings

Roller Bearings come in a number of design variants, adapted to specific applications and operating conditions. The most important criterion for their classification is the shape of the rolling elements, which significantly influences bearing properties, speed range and resistance to axial and radial loads.

Division of Roller Bearings according to the shape of the rolling elements

Ball Bearings
This is the most common type of Roller Bearings. Their rolling elements are balls, which roll between ring raceways. They are characterised by low friction and the ability to run at high speeds. Suitable for moderate radial and axial loads. Available in the following designs, angular, swivel and longitudinal, others are available to suit a variety of applications from domestic appliances to precision machinery.

Ball Bearings

Cylindrical roller bearings
Instead of balls, they use rollers, which ensure linear contact with the raceways. As a result, they have a significantly higher radial load carrying capacity than ball bearings. They are used where, where high loads and high speeds are involved, e.g. in gears, motors and railway axles. Some designs allow for compensation of axial displacement of the shaft relative to the housing.

Cylindrical roller bearings

Cone Bearings
They are characterised by conical rollers and raceways. They carry both high radial loads, and axial loads - especially when acting simultaneously. They are often used in pairs, to allow forces to be transmitted in both axial directions. Tapered roller bearings are used in automotive wheel bearings, agricultural machinery and machine tool spindles.

Tapered roller bearings

spherical roller bearings
Equipped with spherical rolling elements, which allow them to compensate for shaft and housing misalignment (this applies to self-alignment up to approx. 0,5-2° depending on the type). Spherical roller bearings are capable of supporting very high radial loads and moderate axial loads. They are widely used in heavy industry, e.g. in mining and paper machinery.

Spherical roller bearings

Needle roller bearings
A special type of cylindrical roller bearing, in which the rolling elements are much thinner and longer. As a result, they have a high radial load carrying capacity with small radial dimensions. Suitable for applications, where mounting space is limited, e.g. in Joints, automotive transmissions and pumps.

Needle roller bearings

Each of these Bearings types is designed for specific operating conditions, which is why it is important to select the right type of bearing for the application. This ensures maximum performance, reliability and durability of the entire mechanical system.

Division of Roller Bearings according to the direction of the forces to be transmitted

In addition to the shape of the rolling elements, an important criterion for the classification of Roller Bearings is the direction of forces, which they are able to transmit. Depending on their design and application, bearings can be designed for radial loads, axial or a combination of these.

Radial (radial)
Radial Bearings carry loads acting perpendicular to the shaft axis. They are the most commonly used bearings in rotating mechanisms. They can also carry some axial loads, if their design allows them, as in the case of deep-groove ball bearings or some types of cylindrical roller bearings.

Axial (thrust)Axial Bearings are designed to carry forces acting along the axis of rotation. Bearings of this type are used in applications, where loads predominate in the vertical or horizontal direction along the shaft axis, such as. in turntables and thrust units. A distinction is made between thrust ball bearings and cylindrical roller thrust bearings, of which the latter have a higher load carrying capacity.

Thrust Bearings

Mixed
Some bearing designs - such as. angular contact ball bearings or tapered roller bearings - are designed to support both radial and axial forces simultaneously. Depending on the operating angle, they can be used singly or in even arrangements, where one unit accommodates axial forces in one direction, and the other in the opposite direction.

Other design features

In addition to the shape and direction of the forces to be transmitted, bearings also differ in their ability to compensate for mounting errors and in the way they are installed and removed.

Tilting and self-aligning Bearings
Self-aligning Bearings have the ability to self-adjust to shaft and housing misalignment. Their rolling elements run on spherical races, to compensate for small mounting deviations. Self-aligning Bearings, often available as complete units with housings, are used in agricultural machinery, construction and textile machinery, where dynamic shaft deflections occur.

Separable and Inseparable Bearings
Detachable Bearings consist of parts, that can be separately mounted and dismounted, making service and replacement much easier. These include.such as. cylindrical roller bearings, needle and tapered roller bearings. In contrast, non-separable Bearings are designs, in which all components are combined and cannot be mounted separately - typical examples are standard deep-groove ball bearings.

The correct choice of Roller Bearings type should always take into account not only the load direction, but also possible mounting inaccuracies and service requirements. This makes it possible to design a drive train or mechanism, that will operate reliably and efficiently for a long time.

Advantages of Roller Bearings

Roller Bearings have become so widely used primarily because of their performance characteristics. Their construction is designed for maximum operating efficiency, ease of handling and reliability over a long service life.

One of the key advantages of Roller Bearings is their low friction, which translates into significantly lower energy consumption compared to sliding solutions. By rolling the components inside the raceway, it is possible to reduce movement resistance to a minimum, which improves the efficiency of the entire mechanical system. Such characteristics are particularly important in devices operating at high speeds or in applications, where energy efficiency matters.

Another advantage is the standardised dimensions. Bearings manufacturers worldwide use uniform dimensional standards, which facilitates machine design and ensures full interchangeability during servicing. This makes it easy for users to select a suitable replacement without the need for design changes.

The ease of mounting and dismounting is also important. Many types of Roller Bearings can be installed quickly, and their design enables them to be removed without difficulty during maintenance or replacement. In addition, detachable variants are available, which further streamline the servicing process.

Last, last but not least is the high durability. With the right selection and maintenance, roller Bearings can run trouble-free for a long time, even under demanding environmental conditions. Their resistance to wear and the ability to operate under fluctuating loads make them indispensable in modern drive systems and rotating mechanisms.

These properties make Roller Bearings not only efficient, and economical over the long term - both in industrial applications, applications, but also in daily use.

Disadvantages of Roller Bearings

Despite their many advantages, roller Bearings - like any technical solution - also have their limitations, which must be considered when designing and operating equipment. Their effective operation requires specific operating conditions and attention to assembly and the operating environment.

One of the most important limitations is sensitivity to contamination. Even small amounts of dust, moisture or metal filings can lead to rapid damage to raceways and rolling elements. This is why seals are used in many applications, however, their effectiveness depends on the environmental conditions and the quality of the seal itself.

Another factor requiring attention is the need for precision assembly. Roller Bearings operate with tight tolerances, therefore, even minor assembly errors can result in improper operation, increased wear or excessive noise. Tools and procedures must be used, to avoid damage during installation.

A disadvantage of, worth emphasising, is also the sensitivity to overload and mechanical shocks. Although many Bearings are designed to carry heavy loads, sudden impacts or prolonged operation at the limit of endurance can lead to micro-damage, cracks or deformation of rolling elements. In applications exposed to such conditions, bearings with increased resistance should be selected for such applications.

High rotational speeds can present risk of noise and vibration, especially in bearings with greater bearing clearance or unbalanced arrangements, especially in Bearings with larger clearances or unbalanced arrangements. Noise can also be an indication of improper lubrication, wear or an assembly defect.

The table below summarises the most important limitations:

Limitation Potential effects in practice
Sensitivity to contamination Faster wear, damage to raceways and rolling elements
Need for precision assembly Increased resistance, noise, risk of premature failure
Sensitivity to overloads and impacts Deformation, fractures, reduction of durability
Noise and vibration at high speeds Strenuous operation, wear and tear of components, reduced comfort

Although the disadvantages listed can affect the life and effectiveness of Bearings, in most cases, they can be minimised through proper selection, proper mounting and regular maintenance.

Roller Bearings applications - examples of industries and equipment

The versatility of Roller Bearings makes them present in almost every industry and technology, that they are present in almost every branch of industry and technology. From simple household mechanisms, to complex industrial machinery systems, their ability to support loads and provide smooth motion makes them indispensable in many applications, their ability to carry loads and provide smooth motion makes them indispensable in many applications. In this section, we look at examples of their use in different sectors.

In automotive applications Roller Bearings play a key role in ensuring vehicles run smoothly and safely. They are found in wheel bearings, where they support high dynamic loads. They are also found in gearboxes, drive axles, half-shafts and in alternators and coolant pumps. Their presence has a direct effect on the efficiency of drive systems and driving comfort.

In engineering and heavy industry Bearings are used in areas, where heavy loads and high speeds occur. They are used in machine tool spindles, in mechanical gears, electric Motors and in machines for processing metal, wood or plastic processing machinery. Bearings in such environments must be highly durable and resistant to vibration and varying operating conditions.

In household appliances and consumer electronics Roller Bearings can be found in appliances such as washing machines, dryers, hoovers, fans or power supplies. They make it possible for motors to operate quietly and energy-efficiently, and ensure long component life. Their small size and ability to operate at high speeds make them ideal for compact designs, their small size and ability to operate at high speeds make them ideal for compact designs.

In materials handling systems and e-commerce Bearings are an essential component of belt conveyors, drive rollers and warehouse automation modules. They enable the fast and smooth movement of goods in distribution centres, production halls and packaging lines. Low failure rates and the possibility of continuous operation have a direct impact on productivity and operational continuity here.

Roller Bearings perform the same function in each of these industries - reducing friction and transferring loads, ensuring the operational reliability of machinery and equipment. With a wide range of types and sizes, they can be easily adapted to the specific requirements of the application in question.

When to use Roller Bearings instead of Plain Bearings?

The choice between Roller Bearings and Plain Bearings depends on a number of technical factors, operational and environmental factors. Although both types perform a similar function, their characteristics make them, that they perform better in different situations. Roller Bearings are often chosen in applications, where precision is important, durability and energy efficiency.

Roller Bearings are worth using when, when:

  • There is a need to reduce frictional energy losses - Roller Bearings generate significantly less resistance than Plain Bearings, resulting in higher mechanical efficiency and lower energy consumption.
  • System requires operation at high speeds - due to their design and limited contact between components, roller Bearings are better able to cope with high rotational speeds without excessive heat build-up, but this also depends on lubrication, load and materials.
  • Ease of installation and maintenance is important - Standard dimensions, wide availability and ready-to-run units make, roller Bearings assembly is fast and convenient.
  • Long service life under dynamic loads is required - Roller Bearings effectively absorb both radial loads, radial as well as axial loads, making them a good choice for applications with fluctuating operating conditions.
  • Space for lubrication system is limited - many Roller Bearings types are available with factory lubrication, simplifying machine design.

Plain Bearings, on the other hand, may be a better choice for very high static loads, simple systems with oscillating motion or where, where resistance to contamination is important. In practice, however, in most modern applications, it is Roller Bearings that provide better performance and greater reliability (e.g. under very heavy loads, in oscillating operation, where there is no continuous rotation).

Therefore, when designing new equipment or modernising existing mechanisms, it is worth considering the use of Roller Bearings everywhere, where efficiency is important, ease of use and availability of replacements.

How to choose the right Roller Bearings?

The right choice of Roller Bearings is one of the key conditions for reliable and long-lasting machine operation. Proper matching of bearing design to operating conditions minimises the risk of premature failure, reduces service costs and ensures optimum performance of the entire system. Selection should not be based solely on dimensions - a number of technical parameters need to be analysed.

Key selection criteria for Roller Bearings

Loads and direction of forces
The type and value of loads have a direct influence on the choice of bearing type. For mainly radial loads, ball or cylindrical roller bearings are most commonly used. For axial or mixed loads, angular contact bearings are more suitable, spherical roller bearings or tapered roller bearings. It is also necessary to determine, whether loads act on one side, or in both directions.

Rotational speed
Each Bearing has a speed limitation, due to friction and heat dissipation capabilities. At high speeds, low-friction ball bearings are a better choice, while at moderate speeds, cylindrical or spherical variants may be considered.

Environmental conditions
Ambient temperature, presence of dust, moisture or chemicals require special attention. In such cases, it is advisable to use Bearings with suitable seals and lubricants adapted to the operating conditions. In aggressive environments, stainless steel or Protective Coatings bearings work well.

Dimensions and tolerances
Bearings should be selected in accordance with mounting space and design requirements. Inner and outer diameter must be considered, width and type of fit. In precision applications, accuracy classes and internal clearance values are also important, such as standard or increased clearance C3.

Typical errors in the selection of Roller Bearings

Selecting a bearing based on a catalogue alone without a full analysis of the operating conditions can lead to problems in operation. Here are the most common mistakes, to avoid:

  • Underestimation of loads - a bearing that is too weak will not be able to transfer the real forces, this can result in rapid wear or damage to raceways and rolling elements.
  • Failure to consider operating conditions - overlooking aspects such as temperature, the presence of moisture or contamination can lead to corrosion or premature loss of lubrication properties.
  • Incorrect clearance and fit - a bearing fit that is too tight or too loose results in increased resistance to, overheating, noise or shaft misalignment, which worsens the precision of the mechanism.

Bearings selection should be based on the manufacturer's technical data, practice from similar applications and - in case of doubt - on the basis of consultation with an experienced technical advisor. The full potential of Roller Bearings can only be exploited with a considered selection. Use online configurators or manufacturers' catalogues, which facilitate, online configurators or manufacturers' catalogues should be used, which make it easier to make a selection based on load and mounting space.

Maintenance and lubrication of Roller Bearings

Roller Bearings need regular maintenance and lubrication in order to run long and trouble-free, require regular maintenance and adequate lubrication. Even the best-fitting bearing can be subject to premature wear, if it is neglected in terms of maintenance. Proper care not only extends the life of the Bearings, but also reduce the operating costs of the entire machine.

Why is lubrication crucial?

Lubrication in a bearing performs several important functions. First and foremost, it reduces friction between rolling elements and raceways, which reduces wear and heat build-up. In addition, it protects metal surfaces from corrosion, prevents contaminants from entering the bearing and can dampen vibration and noise.

The most commonly used lubricants are:

  • plastic lubricants, which are used in most typical applications. Form a durable protective film, are easy to apply and hold well inside enclosures.
  • Oils, which are used in applications, where there are very high speeds or the need to dissipate heat. They allow more intensive cooling and better flushing of contaminants.

The choice of application method depends on the operating conditions and machine design. Common solutions are manual lubrication via callipers, central lubrication systems, oil bath, splash or oil mist lubrication. Regardless of the method, the key is to maintain the correct lubricant level and check it regularly.

How do you recognise Roller Bearings problems?

A properly functioning bearing should run quietly, smoothly and without noticeable vibration. Any deviation from the norm can be an indication of an incipient fault. The most common symptoms of problems include:

  • excessive noise, which may indicate raceway wear, lack of grease or presence of foreign bodies inside the Bearings,
  • vibration, usually indicating unbalance, damage to rolling elements or improper seating,
  • overheating, which is often caused by excessive load, inadequate clearance or insufficient lubrication.

To avoid failures, regular maintenance is recommended, during which the lubricant condition is checked, the cleanliness of the surfaces and the play and operating temperature of the Bearings. In many applications a preventive maintenance schedule works well, which takes into account the cyclical replenishment or replacement of lubricant and the inspection of rolling elements.

Caring for Bearings does not have to be complicated - you just need to be systematic and follow the manufacturer's recommendations, to ensure their reliability even in difficult operating conditions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

rightColumnPicture rightColumnPicture

READ ALSO