How to safely and effectively remove insulation from electrical wires
How to safely and effectively remove insulation from electrical wires
Date of publication:
14-11-2025
🕒
5
min read
Removing insulation from wires is one of the fundamental tasks in all electrical work – from simple repairs at home to professional installations. Although it seems simple, improper execution can lead to wire damage, and consequently – to connection problems, overheating of the installation, or even short circuits. Therefore, it is worth knowing how to do it correctly and which tools to use so that the work is not only fast but above all safe.
In this article, we will take a closer look at topics such as:
The wire insulation plays a crucial role – it protects the conductor from mechanical damage, moisture, and above all from accidental contact with other wires or conductive elements. If during insulation removal copper or aluminum is damaged, the wire loses its strength, which over time can lead to connection overheating, conductor breakage, or short circuit. On the other hand, leaving a too long exposed section increases the risk of accidental contact and electric shock. Properly performed insulation removal ensures not only user and installation safety but also guarantees durability and reliability of electrical connections.
What tools should you have on hand?
Professional tools are designed to remove insulation precisely and without risk of damaging the conductor. Thanks to appropriately selected jaws or automatic diameter adjustment, the wire can be quickly prepared for installation while maintaining its full strength and conductivity. It also means convenience and time saving – the work is repeatable, precise, and safe.
On the market, many tools for insulation stripping can be identified, including:
Classic insulation stripper (manual stripper) – this is a simple tool used to remove insulation coating from electrical wires. It usually takes the form of pliers equipped with appropriately shaped holes or blades adapted to different cable diameters. It allows quick and precise scoring and removal of insulation without damaging the conductor. This type of tool is lightweight, easy to operate, and requires no additional power. It is suitable both for home tasks and simple installations where occasional wire preparation for joining or soldering is needed.
Automatic insulation stripper(automatic stripper) – one of the most practical and modern tools for insulation removal from wires. Its biggest advantage is self-adjustment to the cable diameter. Just insert the wire into the jaws and squeeze the handles. The tool automatically scores the insulation and strips it off in one smooth motion, leaving the conductor in perfect condition.
Automatic stripper for round and flat wires
Multifunctional pliers – a universal tool that combines several functions – insulation removal, wire cutting, and often crimping cable terminals (so-called ferrules). Thanks to their versatility, they work great in a home workshop where you don’t always have a full set of specialized tools at hand.
Flat cable stripper – a specialized tool designed for removing insulation from two- or three-core cables, often used in lighting installations, RTV equipment, or other household devices. The tool allows simultaneous and even stripping of several conductor cores, significantly speeding up the work compared to stripping insulation one by one.
Cable knife – a basic hand tool used for insulation removal, most often in emergencies or when working with thick cables that do not always fit standard strippers. It comes in various forms – with a hooked, straight, or flat blade, allowing precise scoring of insulation to then remove it.
Cable knife for diameters from 8...28mm
Step by step: how to safely remove insulation?
Safe and proper removal of insulation from electrical wires is one of the basic skills both for professional electricians and DIY enthusiasts performing small repairs at home. Although this task may seem simple, improper execution can lead to wire damage and in extreme cases to short circuits or electric shock. To prevent this, several basic rules should be followed:
Choose the right tool
Selecting the appropriate tool for insulation removal is crucial for the safety and durability of the wire. An unsuitable tool can easily damage the conductor, leading to poor conductivity, overheating, or connection failure.
Set the stripper diameter
Adjusting the stripper diameter is key to safely and effectively remove insulation from the wire. Before using the tool, check the cable cross-section you will be working with. Then set the stripper so that its hole or blade matches the wire diameter – a too small hole may cut or damage the conductor, while a too large one will not evenly score the insulation and make it difficult to remove.
Prepare the wire in the tool and remove insulation
In a manual stripper, adjust the jaws’ hole to the conductor diameter. Then squeeze the handles so that the blades cut only the insulation without damaging the conductor. Pull along the wire to remove insulation in one smooth motion. Check that the conductor strands were not damaged.
In an automatic stripper, insert the wire into the tool jaws. Then squeeze the handles; the mechanism will automatically score and slide off the insulation along the wire. Check that the exposed conductor has the proper length and that the conductor structure remains intact.
When using a cable knife, gently score the insulation along the wire, trying not to cut the conductor. Slide off the insulation with your fingers or pliers, controlling not to damage the conductor. Check that the conductor is undamaged.
Check the wire after removing insulation
This is a very important step where you should ensure that the conductor is whole, unscratched, and undamaged. If you notice micro-cracks or fractures, cut off the wire section and try again. For multi-conductor cables, make sure each conductor is undamaged.
Good practices for insulation removal
Removing insulation from electrical wires seems like a simple task but requires precision and proper preparation in practice. Even small mistakes, such as conductor fractures, too long exposed sections, or using the wrong tool, can lead to weak connections, wire overheating, and in extreme cases, short circuits or electric shock. That is why it is so important to know proven methods, appropriate tools, and good practices that allow you to work quickly, accurately, and above all safely.
Below are some good practices you should follow when removing insulation:
Always disconnect power – safety is paramount.
Choose the right tool – stripper, automatic stripper, or multifunctional pliers.
Set the proper length of exposed conductor – usually 5–10 mm, matched to the connector or terminal block.
Work slowly and precisely – avoid sudden movements and tugging on the insulation.
Check the conductor condition after insulation removal – no part of copper or aluminum should be fractured.
Do not use improvised tools – e.g., kitchen scissors or table knives.
Inspect every conductor in multi-core cables – ensure all are undamaged and evenly stripped.
Regularly maintain your tools
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.
Your credit limit has been exceeded. Your order will be accepted but not realized. The delivery schedule will not be set. Please contact a TME employee.