+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Date of publication: 06-05-2026 🕒 8 min read
The smart home has ceased to be a privilege reserved for the few. Thanks to Raspberry Pi, it is possible to build an advanced home automation system for a fraction of the cost of commercial solutions.
More importantly, the user retains full control over the data and functionality of the system. Unlike the closed ecosystems of Google, Amazon, or Apple, where the system is dependent on corporate privacy policies and often also on monthly subscriptions, the Raspberry Pi-based solution provides real digital independence.
This platform has evolved from an educational tool into the foundation of modern home automation installations. Its universality, support for Linux systems, and the ability to communicate directly with sensors and actuators via GPIO pins make Raspberry Pi capable of integrating technologies that often remain incompatible in the commercial world.
It is a solution that connects old and new systems – analog and digital, simple and advanced – into one cohesive ecosystem operating according to the user's principles.
Home Assistant is an open-source platform that fundamentally changes the way smart devices are managed. Installed on Raspberry Pi, it creates a local home automation hub, integrating products from various manufacturers into one cohesive ecosystem.
Instead of using multiple applications – one for Philips Hue bulbs, another for the Nest thermostat, or yet another for the Xiaomi vacuum cleaner – you get a single control center.
The key difference lies in the system architecture. In traditional solutions, every command goes to external servers and then returns to the device. Home Assistant processes data locally, resulting in a significantly faster response – often below 100ms (instead of several seconds in cloud systems).
Additionally, the system operates even during a complete Internet failure, which is crucial for security functions or heating. Privacy is equally important – data such as camera recordings, presence information, or user preferences remain on the local network and are not sent to external systems.
Home Assistant allows for the creation of advanced automations. For example: when the temperature in the bedroom exceeds 24°C at night, the system will automatically turn on the air conditioning and lower the blinds. Conversely, when the last person leaves the house (based on smartphone locations), the lights will be turned off, heating will be reduced, and the alarm will be activated.
The configuration possibilities are virtually limitless and depend solely on the user's needs.
Every IoT device in the home – from the TV to the refrigerator – can generate network traffic related to analytics, advertising, or telemetry. Pi-hole acts as a local DNS server that intercepts and blocks requests to advertising and tracking servers.
This process is completely transparent to the user and covers all devices on the network – without the need to install additional software on each of them.
Analyzing Pi-hole logs often reveals the scale of the phenomenon. Smart TVs can generate hundreds of connections daily, even in standby mode. Other devices, such as IP cameras or household appliances, can also communicate with external servers in ways that are not obvious to the user.
Pi-hole blocks such connections while speeding up webpage loading by eliminating advertising scripts. In practice, users often observe a significant reduction in website loading times.
The system also allows for the creation of rules for individual devices. For example, access for a smart TV can be restricted to selected services or completely cut off from the Internet while maintaining functionality on the local network.
This solution not only increases privacy but also allows for better control over the security of the entire home network.
Remote management of a smart home requires an appropriate level of security. Exposing router ports directly to the Internet significantly increases the risk of attack – automated bots scan the network for vulnerable services, and hacking attempts can begin almost immediately.
A much safer solution is to use your own VPN server, e.g., based on the WireGuard protocol, running on Raspberry Pi.
WireGuard stands out with its modern and lightweight architecture. It provides:
Once the connection is established, an encrypted tunnel is created between the user's device and the home network. This allows you to access automation systems, cameras, or files just as if you were at home – without the need to expose services externally.
In practice, this means the ability to:
All of this occurs securely – data is encrypted and inaccessible to third parties, including network operators.
Advanced projects using Raspberry Pi enable automatic license plate recognition and access control to properties. In a typical scenario, a sensor (e.g., ultrasonic) detects a vehicle, a camera takes a picture, and the system analyzes the image locally – without the need to send data to the cloud.
The process includes license plate identification, perspective correction, and comparison with a database of stored numbers. If a match is found, the system can automatically open the gate or trigger other scenarios, e.g., notifying the user.
A key challenge is operating in nighttime conditions. This requires using a camera without an IR filter and additional infrared lighting. License plates are designed to reflect IR radiation, allowing for effective reading even in very low light conditions.
The system can also maintain an event log – recording information about vehicle entries and exits along with time and images. Such a solution is applicable not only in private homes but also in small businesses or facilities with controlled access.
In more advanced configurations, it is possible to define security rules, e.g., blocking access for unknown vehicles and automatically sending alerts with images.
The video intercom system based on Raspberry Pi allows for the creation of a fully functional solution without the need to use paid cloud services. Unlike commercial products, the user retains full control over the data and the operation of the system.
When the doorbell is pressed, the system can simultaneously trigger several scenarios: play a voice message at home, send a notification to a smartphone, and provide a live view from the camera with the option to start a conversation.
This allows the user to remotely check who is at the entrance, talk to the guest, or – if necessary – open the door, regardless of their location.
This solution works well in both everyday situations and during the absence of household members. It allows, for example, to provide instructions to a courier or control access to the property without physical presence.
Maintaining a reef aquarium requires very precise control of environmental parameters. The Reef-Pi project allows Raspberry Pi to be transformed into an advanced aquarium management system, competitive with commercial solutions.
The system enables control of key parameters such as temperature, water level, and lighting. By integrating with sensors and actuators, it is possible to maintain stable conditions necessary for marine organisms.
One of the critical processes is compensating for water evaporation. In marine aquariums, this leads to increased salinity, which can be dangerous for corals. Liquid level sensors can automatically activate dosing pumps to add water in precise amounts, restoring the appropriate balance.
The system also allows for lighting control using PWM signals, enabling the replication of the natural day and night cycle. This directly impacts the health of organisms and the stability of the ecosystem.
In more advanced configurations, it is also possible to dose supplements and conduct continuous monitoring of parameters. Data is recorded in real-time, allowing for trend analysis and quick responses to potential problems.
Automatic irrigation systems based on Raspberry Pi can significantly increase the efficiency of watering plants, provided that appropriate sensors and control logic are used.
In practice, capacitive sensors work best, as they do not wear out quickly compared to resistive models. Their design eliminates current flow through the soil, preventing corrosion and ensuring stable measurements over a longer period.
The system can monitor soil moisture in different zones of the garden and also take into account external data such as weather forecasts. This ensures that watering occurs only when truly needed – e.g., it will not be activated just before expected rain.
It is also possible to adjust the amount of water to specific plants and environmental conditions. More advanced configurations utilize additional sensors to monitor parameters such as temperature or sunlight, allowing for even more precise irrigation control.
In practice, this means not only water savings but also better growth conditions for plants and a reduced risk of damage due to drying out or overwatering.
The PZEM-004T module is a measurement circuit that communicates with Raspberry Pi via a serial interface. Unlike simple current sensors, it allows for simultaneous measurement of voltage, current, and calculation of actual energy consumption.
The device also allows for determining additional parameters such as power factor or network frequency, providing a fuller picture of the electrical installation's operation.
The measurement is performed non-invasively – using a current transformer mounted on the wire, without the need to cut it. Additionally, the measurement part is galvanically isolated from the 230V network, increasing the safety of the entire system.
Collected data can be recorded and analyzed in real-time, e.g., in the form of graphs. This makes it easy to identify devices generating excessive energy consumption, including so-called "energy vampires" that operate in standby mode.
In practice, the system enables precise analysis of operating costs – e.g., comparing energy consumption by different devices or detecting anomalies that may indicate an impending failure.
It is also possible to define alarm thresholds. If these are exceeded, the system can automatically send a notification, informing about, for example, a device left on.
A popular solution in smart home projects is the use of Wi-Fi sockets with alternative firmware, such as Tasmota. This allows for full integration with Raspberry Pi and communication using the MQTT protocol.
As a result, sockets can become part of more complex automation scenarios. For example, detecting an increase in power consumption by the TV can automatically trigger specific actions – e.g., dimming the lights, lowering the blinds, or changing the settings of other devices in the room.
The system can also serve a protective function. In the case of prolonged energy consumption – e.g., by a charger left in the socket – it is possible to automatically cut off power. This helps reduce energy consumption and minimize the risk of overheating devices.
Such solutions demonstrate that even simple elements of electrical infrastructure can become part of an advanced and fully automated home management system.
Raspberry Pi can support the automation of many daily activities, increasing the comfort of home use and eliminating repetitive tasks.
An example could be projects for automatic pet feeders. The control system dispenses food in specified portions and at set times, ensuring repeatability and control over the feeding process.
In more advanced projects, it is also possible to verify the operation of the system – e.g., using a camera – and collect data to monitor the pet's behavior.
Such solutions show that home automation can encompass not only technical systems but also everyday, practical aspects of life.
Raspberry Pi can also be used to control a height-adjustable desk, supporting work ergonomics and healthy habits.
The system can monitor user activity – e.g., based on computer work time, data from presence sensors, or integration with a calendar. Based on this, it is possible to automatically adjust the desk position.
For example, after a specified period of sitting work, the system may suggest a position change and raise the desk to standing mode. If inactivity or a change in work context is detected, the settings can be automatically adjusted.
More advanced configurations allow for considering additional data, such as meeting schedules or information from wearable devices. This enables the system to better tailor its operation to the user's actual work mode.
This solution demonstrates that home automation can support not only comfort but also health and work efficiency.
The Magic Mirror project combines the functionality of an information system with the aesthetics of a modern interior. A monitor placed behind a one-way mirror displays content in such a way that it appears to float on its surface.
The system can present the most important information in real-time – weather forecasts, calendars, news, or public transport data. This provides the user with quick access to key information without the need to reach for their phone.
Magic Mirror can also be integrated with the home automation system. This allows for displaying notifications such as device status, delivery information, or system alerts.
This solution exemplifies the combination of technology with everyday functionality, offering convenient access to information in a natural place – in front of the mirror.
One of the key challenges in designing a smart home system is integrating automation with traditional light switches. Users expect the installation to work both automatically and in a classic manner – without the need to reach for an app.
There are several approaches to solving this problem.
The simplest involves using a relay as a parallel element to the traditional switch. This solution provides full manual functionality, but the system does not have direct information about the current state of the lighting. This issue can be partially resolved by using additional sensors.
An alternative is monostable switches that act as buttons controlling the system. In this case, Raspberry Pi manages the entire process, ensuring it always knows the state of the lighting. However, the downside is the dependency on the system's operation – in case of failure, control may be limited.
The most advanced solution involves smart switches that communicate wirelessly, e.g., in Zigbee or Z-Wave standards. They combine manual functionality with full system integration, offering the greatest flexibility but also a higher implementation cost.
The choice of the appropriate solution depends on the user's requirements and the level of reliability to be achieved.
Raspberry Pi opens new possibilities in building smart home systems, offering full control over data, great flexibility, and independence from closed ecosystems of manufacturers. Solutions based on local data processing eliminate the need to use cloud services and help avoid additional subscription costs.
The system can operate independently of Internet access, and its development depends solely on the user's needs. This approach is particularly gaining importance in the context of growing awareness regarding privacy and data security.
Building your own home automation system is not only a matter of convenience but also an investment in technical skills. Working with Raspberry Pi develops skills in electronics, programming, and computer networks, which are applicable beyond the home environment.
It is also worth noting the development of standards such as Matter, aimed at ensuring interoperability of devices from different manufacturers. This direction aligns with the philosophy of open systems – based on local data processing, transparency, and user control.
As a result, Raspberry Pi remains one of the most versatile tools for building a smart home – both for hobbyists and more advanced users.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.