+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Chisel - definition

Chisel is a hand tool used in material processing by cutting, shaping, carving, or making indentations in various surfaces such as wood, metal, stone, or plastics. Its construction includes a working part in the form of a sharp cutting edge and a handle, allowing precise guidance and control of pressure or blows with a hammer or mallet. The cutting part of the chisel is usually made of hardened tool steel with high resistance to wear and deformation, ensuring durability and stability of the blade geometry during intensive use.

The profile of the chisel's cutting edge can take various forms depending on its purpose: from simple, flat blades used in carpentry to specialized semi-circular, oblique, or V-shaped forms used in sculpture and woodcarving. In mechanics and locksmith work, metal chisels are used for machining materials with high hardness, such as steel or brass, where both high blade strength and impact resistance are necessary.

In modern manufacturing technologies, chisels undergo precise grinding and heat treatment processes to ensure a uniform material structure and optimized performance properties. Proper technique when working with a chisel includes both the appropriate selection of the angle of attack and control of the impact force to achieve high-quality surface finish and maintain operator safety. In industrial and artisanal applications, chisels remain an indispensable tool, enabling the execution of precise machining operations with high-quality requirements.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO