+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Photoelectric cell (phototube) - definition

Photoelectric cell (phototube) is an optoelectronic component used to detect the presence of light or changes in its intensity, functioning as a sensor in various automation, security, and control systems. Its operation is based on the photoelectric effect, in which electromagnetic radiation—typically in the visible or infrared range—induces the generation of an electrical signal when it strikes a semiconductor material. Depending on the design and applied technology, a photoelectric cell can respond to continuous, pulsed, or modulated light.

A typical photoelectric cell consists of a transmitter that emits a light beam and a receiver that detects the interruption, attenuation, or reflection of the beam caused by the presence of an object. This system operates without physical contact, enabling rapid and precise detection of moving objects or environmental changes without direct interaction with the monitored element. As a result, photoelectric cells are widely used in safety systems, industrial automation, transport devices, light barriers, and motion-controlled lighting systems.

The advantages of photoelectric cells include high sensitivity, fast response time, and the ability to operate in harsh environmental conditions such as dust, vibration, or variable lighting. Their technical parameters can be tailored to specific applications by selecting appropriate wavelengths, detector types, and signal processing methods. In modern systems, photoelectric cells are often integrated with microcontrollers, enabling advanced data analysis, interference filtering, and seamless integration with other components of intelligent installations.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO