+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Amplidine - definition

Amplidine is a type of electromechanical amplifier, used mainly in control and regulation systems, especially in the days before the development of modern electronics. It is based on the operating principle of a direct current generator with the excitation winding controlled by a low-current input signal, which allows much higher output currents to be precisely controlled.

From a technical point of view, an amplifier is a specially designed alternator with additional control and compensation windings, which converts a small input signal power into a much higher output power. In this circuit, strong magnetic coupling between the control circuits and the main output circuit plays an important role, this results in a high power amplification effect.

A characteristic feature of the amplifier is its ability to maintain stable operation under heavy loads and its resistance to interference, making it useful in Servo Motors systems, industrial automation and military fire control systems in the mid-20th century. In a typical configuration, it was used to amplify a voltage signal to control DC motors, where reliability and the ability to precisely control high power outputs were crucial.

Although amplifiers have now been almost completely replaced by solid-state amplifier circuits, their historical importance for the development of control technology and electrical power engineering remains significant. They are an example of mechanical-electrical-electrical amplification systems, which, in their time, made it possible to implement complex control functions without the use of digital electronics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO