+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Autotransformer - definition

Autotransformer is a type of electrical transformer in which the primary and secondary windings form a common, physically connected coil, and the voltage difference between the input and output sides is achieved through appropriate taps on the same winding. Unlike a transformer with two separate windings, an autotransformer has only one winding, which affects its design, cost, and energy efficiency.

Thanks to the common winding, the autotransformer is characterized by a smaller mass and volume for the same rated power compared to a classic two-winding transformer. This is because part of the energy is transferred directly through electrical conduction, not solely through electromagnetic induction. Such a construction also allows for higher efficiency and better voltage regulation parameters with small differences between input and output voltage.

Autotransformers are used in applications where galvanic isolation between the primary and secondary sides is not required. They are used, among others, in motor starting systems, laboratory equipment, for voltage regulation, and in power networks for voltage transformation in the medium and high range. Their use is limited by the lack of insulation between circuits, which involves the risk of transferring disturbances or overvoltages, so their use requires careful analysis of operating and safety conditions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO