+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Data block - definition

A Data Block is the basic organisational unit of information used in computer systems to store, transmit and process data. It represents a defined, logically consistent portion of fixed or variable length information that is treated as a whole in the context of disk operations, network transmissions or memory management.

In file systems, a data block is the smallest portion of data that a system can physically store on a storage medium, e.g. a hard disk or SSD. The size of this block - the so-called system block size - affects the efficiency of disk space use and the speed of I/O operations. Too large a size can lead to wasted space (so-called internal fragmentation) and too small a size can lead to excessive I/O operations.

In operational memory, data blocks are important for resource management by the operating system, especially in the context of memory allocation and release, or in the operation of caches. In Computer Networks, a data block can represent a segment transmitted within a communication protocol frame, where it contains user information and control data such as headers, checksums or identifiers.

In the context of databases and programming, a data block is sometimes a logical structure, containing a set of records, variables or pointers used during data writing, reading and processing operations in memory or on disk. In many systems, such as PLCs or embedded systems, the term refers to an ordered address space with input, output or temporary data processed by control applications.

The data block is therefore a universal concept in computer science and digital electronics, relevant to the efficiency of systems, data integrity and logical ordering of data.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO