+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Shunts - definition

The Shunts is a precision measurement resistor used in electrical systems for controlled current distribution and precise measurement of current values in circuits high-current. Its operation is based on the principle of proportional relationship between the current flowing through conductor and the voltage drop across its terminals, according to Ohm's law. The design of the shunt allows a significant portion of the current to be routed through a resistor with a precisely defined, low resistance value, making it possible to obtain a measurable voltage proportional to the current without significantly affecting the electrical parameters of the circuit.

The material used in the construction of the shunt must have a low temperature coefficient of resistance, which ensures measurement stability even at high current values. Feet used for its manufacture are manganese, constantan or nickel-chromium alloys, which are characterised by minimal change in electrical resistance as a function of temperature and high resistance to material ageing. The structure of the shunt is designed to effectively dissipate the heat generated during high current flow, thus reducing temperature drift and extending the life of the component.

In measurement systems, the shunt is used in conjunction with analogue and digital meters, where the voltage measured at its terminals is converted to a current value by Operational amplifiers, analogue-to-digital converters or microprocessor systems. Shunts are often calibrated in precision configurations to minimise measurement errors and compensate for unwanted thermal and electromagnetic effects.

In protection systems, shunts act as current limiting and control elements in power circuits, enabling the implementation of overcurrent protection mechanisms and dynamic monitoring of energy consumption. High-current shunts with high load capacity are used in industrial and power applications, used in electrical network monitoring systems, energy storage and control systems for electric actuators.

Shunts' integration with modern telemetry systems and IoT systems allows for remote diagnostics of electrical loads, analysis of machine operating parameters and real-time optimisation of energy consumption. Shunts with a layered structure, manufactured using precision thin-film processing methods, are used in solutions that require miniaturisation, allowing their implementation in advanced measurement systems and integrated circuits used in automotive and aerospace electronics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO