+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Voltage divider - definition

A Voltage Divider is a basic electrical circuit used to proportionally reduce the input voltage relative to the supply voltage. It usually consists of two or more passive elements, most commonly resistors, connected in series, although in some cases capacitive or inductive components may also be used, depending on signal characteristics and application requirements.

The principle of the divider is based on Ohm's law and the voltage division rule in a series circuit. The total voltage applied to the circuit is distributed between its elements according to their resistances. The output voltage drawn from an intermediate point between these elements is a function of the ratio of their resistances, allowing the desired voltage value to be precisely obtained within a specified range.

The voltage divider is widely used in measurement, control and analogue systems where there is a need to match signal levels, scale input or reference voltages and produce reference voltages. It is also used in digital electronics to convert logic levels between different voltage standards.

When designing voltage dividers, the effect of the load on their characteristics must be taken into account, as connecting a low-impedance load to the measuring point can disturb the voltage ratio and introduce unwanted deviations. In cases requiring high accuracy, signal buffering or the selection of components with a sufficiently high impedance value is used.

Although the principle of the divider is simple, its correct implementation requires consideration of a number of practical factors such as resistor tolerances, temperature effects, noise and parameter stability over time. In dynamic applications, capacitive dividers are also used, which are analysed in the frequency domain using the complex impedance.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO