+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
An Estimator is a mathematical function or rule used to determine the approximate value of an unknown population parameter from available sample data. In mathematical statistics, the estimator acts as an inferential tool to move from empirical data to inferences of a general nature. Its value obtained for a particular sample is called an estimate, and the estimator itself has the character of a random variable, since it depends on the randomness of the sample.
The performance of an estimator is judged by its statistical properties, such as unconstrainedness, consistency, efficiency and minimum variance. An unconstrained estimator gives on average correct results, a consistent one converges to the true value as the number of observations increases, and an efficient one makes maximum use of the available information in the data. Many applications seek to construct estimators that minimise mean squared error or meet optimality criteria according to estimation theory.
In engineering, estimators find applications in measurement systems, adaptive control, filter theory and signal processing. An example is the Kalman filter, which is a dynamic state estimator used to track system parameters based on time series with noise and measurement noise. In robotics, Automation and navigation systems, estimators are used to determine the position, velocity or orientation of objects under data uncertainty.
In computer science and machine learning, estimators appear as elements of regression and classification algorithms for generalising patterns from training sets. Their construction can be based on parametric, Bayesian, frequentist or non-parametric methods, depending on the model assumptions made. Correct interpretation and use of estimators requires an understanding of their limitations, dependence on data distributions and the impact of measurement errors and noise on the quality of estimates.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.