+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Perfect gas - definition

A Perfect Gas is an idealised model of a gaseous substance in which the gas molecules are assumed to be point-like objects that do not interact other than through elastic collisions. Its description is based on the kinetic theory of gases and the equation of state of a perfect gas, which defines the relationship between the pressure, volume and temperature of a substance under thermodynamic conditions.

The basic assumption of the perfect gas model is that there are no intermolecular forces, which means that the potential energy of interactions between molecules is negligible relative to their kinetic energy. Particle motion is random and collisions occur according to the principles of conservation of momentum and energy, leading to a uniform distribution of particle velocities according to the Maxwell-Boltzmann distribution.

The Clapeyron equation, which is the mathematical treatment of a perfect gas, expresses the relationship:

PV = nRT

where P is the pressure, V the volume, n the number of moles of the gas, R the universal gas constant and T** the temperature expressed in the Kelvin Scales.

The perfect gas model allows for a simplified description of thermodynamic processes such as isothermal, isobaric, isochoric and adiabatic gas transformations in which the state parameters change according to specific mathematical relationships. In technical thermodynamics, the perfect gas forms the basis for the analysis of heat engine cycles, gas turbines and refrigeration systems, where approximate equations of state allow the efficiency of energy processes to be predicted.

The internal energy of a perfect gas depends solely on temperature and is determined by the ability of the molecules to store kinetic energy in the form of translational, rotational and oscillatory motions. In the case of mono-atomic gases, such as helium and neon, the kinetic energy is exclusively related to translational motion, whereas in multi-atomic gases the additional degrees of freedom lead to an increase in the heat capacity of the gas.

The perfect gas model is used in mechanical engineering, aerodynamics, the chemical industry and astrophysics to analyse gases at high temperatures and low pressures, where the molecular interactions are so weak that the actual gas behaviour approaches the theoretical description of a perfect gas. Under high pressure or low temperature conditions, when gas molecules start to interact due to van der Waals forces, it becomes necessary to use more complex models, such as the van der Waals equation of state or real gas models describing compressibility and phase condensation effects.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO