+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Hadron - definition

The Hadron is a complex particle subject to the strong interaction - one of the four fundamental forces in physics. It is made up of quarks that are permanently bound by gluons according to the principles of quantum chromodynamics (QCD). Hadrons are divided into two main groups: baryons, consisting of three quarks (e.g. protons and neutrons), and mesons, which are quark-antiquark systems. Unlike elementary particles, hadrons have an internal structure and are susceptible to decay under appropriate energy conditions.

From the point of view of particle physics, hadrons play a fundamental role in the description of nuclear matter. Protons and neutrons, as baryons, form atomic nuclei, which are the basis for the existence of visible matter. Although mesons are unstable and usually occur as products of high-energy processes, their study provides valuable information about the nuclear force and quark dynamics.

The properties of hadrons, such as mass, electric charge, spin or lifetime, result from the configuration of quarks and their interactions. Hadrons cannot exist in isolation as single quarks - they always form colour-neutral systems according to the confajnment principle. This distinguishes them from leptons, which are not subject to strong interactions.

Modern experimental physics, including experiments conducted at particle accelerators, such as the Large Hadron Collider (LHC), focuses on analysing reactions involving hadrons, searching for new types of hadrons and testing theoretical models describing the structure of matter at the subatomic level. This research allows a better understanding of the mechanisms responsible for the stability of atomic nuclei and the evolution of the Universe.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO