+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Heatspreader - definition

A Heatspreader is a passive component used in electronic designs to efficiently distribute heat generated by semiconductor components such as processors, memory chips, power transistors or LED modules. Its main function is to increase the surface area of heat dissipation, allowing for even temperature distribution and reducing local overheating points that could adversely affect device durability and performance.

Heatspreaders are made from materials with high thermal conductivity, most commonly copper, aluminium or their alloys. Their design can take the form of flat wafers, guards or specially moulded components integrated into the IC chassis. In many cases, they are directly connected to the surface of the heat source using materials that improve thermal conductivity, such as pastes, washers or phased thermal connectors.

Unlike a classic heatsink, whose function is to dissipate heat to the environment, a heatspreader acts mainly as an intermediary - transporting heat from a point source to a larger contact area, often working in conjunction with more advanced cooling systems. Thanks to its design, it helps to reduce temperature gradients and increase the efficiency of the heat exchange in the downstream cooling stages.

Heatspreader technology is particularly important in high power density devices where traditional cooling methods prove insufficient. Their proper design has a direct impact on the reliability of electronic circuits and meeting thermal requirements in industrial, consumer and military applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO