+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The SD (Secure Digital) card is a compact Mass Storage media based on flash memory technology, designed to store and carry digital data in electronic devices. The standard was developed in 1999 by a consortium of SanDisk, Panasonic and Toshiba, and its specification defines both the physical dimensions of the card and the communication protocols and data protection mechanisms.
Memory Cards use NAND flash memory chips, working with an on-board controller that manages write, read and error correction processes through mechanisms such as ECC (Error Correction Code) and wear leveling, which extend memory life. This technology allows high capacity to be achieved while maintaining a compact size and low power consumption.
Over time, developments of the standard have been introduced, such as SDHC (Secure Digital High Capacity), SDXC (Secure Digital Extended Capacity) and SDUC (Secure Digital Ultra Capacity), enabling storage of data sizes of up to several terabytes. The performance of SD cards is determined by speed classes such as Speed Class, UHS Speed Class and Video Speed Class, defining minimum guaranteed write speeds, which is important for applications requiring constant and fast data transfer, such as high-definition video recording or serial photography.
SD cards have found their way into a wide range of devices, from cameras and video cameras, to mobile phones and tablets, to drones and embedded systems. Due to their versatility, mechanical robustness and capacity scalability, Memory Cards are one of the most widely used portable memory formats in modern consumer and industrial electronics.
MicroSD card connectors]{.cs-center}
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.