+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Reed Sensors is an electromechanical electrical switch, whose operation is based on the phenomenon of magnetic attraction. It consists of thin, flexible metal contacts placed inside a hermetically sealed glass tube. The contacts are made of ferromagnetic materials and, in the absence of a magnetic field, remain open or closed - depending on the design. Approaching an external magnetic field source, such as a permanent magnet or solenoids, causes them to attract and change their conductive state.
By being encapsulated in a vacuum or inert gas atmosphere, Reed Sensors have a very high mechanical durability and resistance to sparking, allowing them to be used in environments with a higher risk of ignition. The response time of Reed Sensors is short, and its design without active parts means that the device does not consume energy when at rest. Its operation is two-state, making it an ideal component for detecting the presence or position of moving parts.
Reed Sensors are used extensively in security systems, especially in door and window opening sensors, as well as in industrial automation systems, liquid flow counters, measurement systems and control devices. Due to their simplicity and high reliability, they are a competitive alternative to more complex electronic sensors, especially where a non-contact, permanent sensing solution is required.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.