+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Quantisation - definition

Quantisation is the process of converting continuous signal values into discrete values, mainly used in the field of digital information processing. It involves mapping an infinite set of possible values of an input signal into a finite set of digital representations, allowing data to be stored and analysed in digital systems. This process is an inherent step in analogue-to-digital conversion, following sampling of the signal.

In mathematical terms, quantisation involves rounding off the values of the signal samples to the nearest acceptable levels, resulting in a quantisation error - the difference between the actual signal and its digital representation. The magnitude of this error depends on the number of quantisation levels and therefore on the resolution of the converter and the recording format used. The greater the number of bits per sample, the higher the representation accuracy, but also the greater the memory and processing power required.

Others are quantisation in various fields of technology, including audio and image coding, communication systems and numerical modelling. In the context of signal processing, techniques to minimise quantisation distortion, such as dithering, are of particular importance to reduce subjectively perceived distortion. In engineering applications, quantisation represents a trade-off between mapping precision and system resource efficiency.

In modern algorithms artificial intelligence and computer graphics, this process is sometimes also used to reduce data dimensions or compress model parameters, which promotes their optimisation under conditions of limited computing power, as is the case in embedded devices.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO