+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
An Arc Lamp is a light source that operates on the principle of an electric arc, formed between two electrodes, usually made of carbon or heat-resistant metals. The light emission results from the intense heating of the electrode material and the ionisation of the gas present in the arc gap. This phenomenon occurs as a result of the application of a voltage sufficient to cause an electrical breakthrough, which initiates and sustains an arc at a very high temperature, reaching several thousand degrees Celsius.
The first arc lamps operated in open air, but over time controlled atmospheres, such as argon, neon or mercury vapour, were used to increase light output and prolong life. Depending on the gas used and the design, arc lamps can emit light with different colour and spectral characteristics. In high-pressure versions, such as the mercury vapour or xenon lamp, intense white or daylight-like light emission is achieved.
Due to their high brightness and focused luminous flux, arc lamps were commonly used in film projectors, stage spotlights, lighthouses and industrial lighting systems. They were also used in arc welding technology and in some chemical processes where an intense heat source was essential. However, their operation involves high power consumption, UV emissions and the need for arc stabilisation and cooling systems.
In terms of design, the arc lamp requires a specialised ignition and current control system, as the arc characteristics are non-linear and unstable without adequate constraints. Although it has been largely superseded by more modern light sources such as discharge lamps and LEDs, it is still sometimes used in specialist applications where extreme light intensity is required.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.