+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Luminescence - definition

Luminescence is the phenomenon of the emission of luminous radiation by a substance under the influence of the absorption of energy, this process not being due to the high temperature of the body as in the case of incandescence. Unlike thermal radiation, luminescence occurs due to transitions of electrons from excited states to lower energy states, during which energy is released in the form of photons.

Others may be caused by different excitation mechanisms, such as absorption of electromagnetic radiation, chemical reactions, the action of an electric field, biological phenomena or particle bombardment. Others distinguish different types of luminescence depending on the source of excitation, including fluorescence, phosphorescence, electroluminescence or bioluminescence. Each of these processes is characterised by a different emission duration and mechanism of return to the ground state.

In technical applications, luminescence is used in display technology, optoelectronic sensors, light sources, medical diagnostics and marking materials, among others. In solid state physics and quantum chemistry, the phenomenon allows the analysis of the electron structure of molecules and the properties of semiconductor materials. Luminescence is also the basis of light-emitting diodes (LEDs), semiconductor lasers and phosphors used in lamps and screens.

Luminescence characteristics, such as the wavelength of the emitted light, intensity, quantum yield and emission duration, depend on the material's physicochemical properties and environmental conditions. Studying these parameters allows luminescent materials to be fine-tuned for specific technological and scientific applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO