+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Magnetostatics - definition

Magnetostatics is the branch of electromagnetism concerned with the study of magnetic fields produced by time-fixed, stationary electric currents. Unlike electrodynamics, where time-varying electromagnetic phenomena are analysed, magnetostatics assumes that the currents are constant and the magnetic field does not change over time, which simplifies mathematical descriptions and allows the use of Maxwell's static equations.

Within magnetostatics, the key is Biot-Savart's law, which allows the calculation of the magnetic induction vector at a given point in space as the result of integrating the effect of elementary currents. The second fundamental tool of analysis is Ampère's law, which relates the circulation of the magnetic field vector around a closed loop to the current flowing through its interior. In engineering applications, magnetostatics enables the modelling and design of structures where magnetic field distributions under steady-state conditions are important.

Magnetostatic phenomena are found, among others, in the magnetic circuits of transformers, motors, Coils and Solenoids, as well as in ferromagnetic materials, where the description of magnetic domains and their interactions can be considered in static terms. Numerical methods, such as the finite element method (FEM), are used in computational engineering to analyse complex three-dimensional systems, taking into account material nonlinearities and boundary conditions.

Magnetostatics does not take into account electromagnetic radiation or electromotive induction, making the model particularly useful in situations where the temporal variation of the field is negligible. Static magnetic field analysis also plays an important role in engineering diagnostics, sensor design and electromagnetic protection.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO