+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Zip drive - definition

The Zip Drive was a type of removable disk drive developed by Iomega in the mid-1990s for storing and transferring computer data. The device used special magnetic media - Zip drives - enclosed in plastic enclosures that looked like an enlarged floppy disk, but offered much higher capacity and data transfer speeds. Depending on the version, Zip disks could hold 100 MB, 250 MB or 750 MB of information, which was a significant advance over standard 3.5" floppy disks.

Zip technology was based on a magnetic recording method similar to that used in hard disk drives, allowing for higher recording density and mechanical reliability. Actuators were available in both internal (PC-mounted) and external versions, connected via interfaces such as SCSI, IDE, USB or LPT. This allowed them to be used with a variety of system platforms, including PCs and Macintosh computers.

Actuators gained popularity in office, education and graphics environments where there was a need to securely transport large file sizes, e.g. DTP projects, data archives or backups. Its advantages included portability, greater mechanical durability than floppy disks and a relatively low running cost. However, over time it has been superseded by more capacious and convenient media such as CD-Rs, DVDs, USB sticks and external disks.

Technological limitations such as susceptibility to mechanical failure and the so-called 'click of death' - a problem found in some models - contributed to a gradual decline in user confidence and the eventual withdrawal of Zip Actuators from the market. Despite this, these devices played an important role in the evolution of Mass Storage during the transition period between the floppy disk era and today's semiconductor-based solutions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO