+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Stress is a physical quantity describing the internal forces acting in a solid that result from the application of external mechanical, thermal or other loads. It is a measure of the intensity of the interactions between the particles of a material against its deformation and is defined as the internal force per unit area of the cross-section through which the force passes. Stress is tensor in nature, which means that its full description requires consideration of both the direction of the forces and the orientation of the cross-sectional plane.
Others in continuous mechanics distinguish between different types of stress, including normal (perpendicular to the cross-sectional surface) and tangential (parallel to the cross-sectional surface), which can occur as uniaxial, biaxial or triaxial stresses, depending on the geometry and type of loading. In addition, the stress state can be characterised by principal stresses, corresponding to the extremes of the principal stress tensor.
The analysis of stress distributions in solids is crucial in mechanical engineering, construction, aerospace and materials science, as it enables the assessment of strength, stiffness and reliability of structures. Exceeding stress limits leads to phenomena such as plasticity, fracture or material creep. Stresses are calculated analytically within the framework of elastic theory or determined numerically using the finite element method (FEA), and in real conditions can be measured using resistance strain gauges, photoelastic methods or interferometric techniques.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.