+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Nuwistor - definition

The Nuwistor is a miniature electron tube, a development of the classic vacuum tubes, developed in the 1950s by RCA as a response to the need for miniaturisation and improved performance of high-frequency electronic circuits. Unlike traditional glass tubes, nuvistors had a metal-ceramic housing, characterised by high mechanical-thermal strength, performance stability and resistance to external influences such as vibration and temperature changes.

Due to their compact size and good electrical properties in the VHF and UHF range, the nuvistors found applications in professional radio equipment, radars, amplifiers and measurement equipment, especially where low noise and high reliability were required. They were characterised by short heating times cathode, high vacuum quality and good linearity, which made them competitive with the first generations of Transistors, which initially failed to match their performance in microwave applications.

Despite their advantages, nuvistors were gradually supplanted by evolving semiconductor technologies that offered even smaller sizes, lower operating voltages and greater ease of integration into integrated circuits. However, during the transition period between the tube and semiconductor eras, they represented an important step towards miniaturisation of electronics and enhanced the development of precision analogue systems, especially in the field of high-frequency technology. Today, nuvistors are of interest mainly to collectors and historians of electronic technology.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO