+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
An Electron Lamp is a vacuum electronic component that controls the flow of electrons between electrodes located in a sealed glass or metal bulb. Its operation is based on thermionic emission - a phenomenon involving the release of electrons from the heated cathode, which then move towards the anode under the influence of an applied voltage. Depending on the number and arrangement of electrodes, the tube can act as a rectifier, an amplifier, an oscillator or a switch.
The basic type of electron tube is the diode, containing only a cathode and an anode. As technology has developed, more complex designs have been developed, such as triodes, tetrodes and pentodes, which allow more advanced control of the signal by adding control grids. Thanks to their non-linear properties and ability to operate over a wide frequency range, electron tubes have been key components in telecommunications systems, Measuring Instruments, radios and televisions for Decades.
The electron tube has a high resistance to overvoltage and the ability to operate at high voltage, allowing it to be used in high-power devices such as high-end audio amplifiers, radio transmitters and industrial high-frequency generators. Although it was largely displaced by Semiconductors in the second half of the 20th century, it remains irreplaceable in some applications due to its unique acoustic, dynamic and thermal properties.
Historically, the development of electron tubes is the foundation of modern electronics. They were the first active components capable of amplifying electrical signals, which ushered in the era of analogue and digital electronics. Their operating principle is based on the classical physics of electrons in a vacuum, before the large-scale introduction of semiconductor technologies.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.