+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Tetrode - definition

The tetrode is a four-element electron tube, which is a structural development of the triode, used mainly in radio technology, amplifiers and high-frequency systems. Its construction is based on the presence of four electrodes: a cathode that emits electrons, an anode that collects charge, and two grids - a control grid and a shield grid - placed between the cathode and anode. An additional grid, called a shielding grid, has been introduced to eliminate unwanted electrostatic interactions between the anode and the control grid, which significantly improves the operating stability and amplification performance of the tetrode compared to triodes.

The shielding grid, located between the control grid and the anode, is usually connected to a positive potential and acts as a barrier to limit the influence of the anode's electrostatic field on the electron flow control area. This reduces the phenomenon of feedback, which in triodes can lead to oscillations and deterioration of amplification linearity. This design allows tetrodes to achieve higher voltage gain and operate at higher frequencies.

However, tetrodes are not free from disadvantages. The most serious of these is the phenomenon of secondary electron emission - a situation where electrons striking the anode knock secondary electrons out of the anode, which can be attracted by the shielding grid. This leads to the phenomenon of the so-called 'dynatronic region' in the characteristics of the anode, manifested by non-linearity and a decrease in the anode current when the anode voltage increases. For this reason, tetrodes have been replaced in many applications by pentodes, which contain an additional grid to prevent secondary emission.

Although semiconductor components have displaced electron tubes in most applications in modern electronics, tetrodes are still used in specialised areas such as broadcast technology, high-end audio amplifiers, or military and laboratory equipment, where their characteristics are still valued.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO