+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Radio transmitter - definition

A Radio Transmitter is an electronic device used to generate, modulate and emit electromagnetic waves in the radio frequency range that enable the wireless transmission of information over a distance. The main task of a transmitter is to transform an information signal - such as sound, images, digital data or a control signal - into the form of a high-frequency signal capable of propagating through space via an antenna.

The transmission process begins with the generation of a carrier wave by an oscillator, whose parameters - most commonly amplitude, frequency or phase - are then modulated according to the waveform of the input signal. The modulated signal is amplified in a power stage and directed to an antenna, which transforms the electrical energy into electromagnetic waves that propagate in the environment. The choice of operating frequency, modulation type and output power depends on the intended use of the transmitter and the applicable regulatory provisions.

Radio transmitters are used in a wide range of applications - from public and commercial communication systems such as broadcasting, television and mobile telephony to satellite transmissions, aerospace, military and automatic control and data transmission systems. Depending on the application, they can take the form of complex transmitter installations or compact modules integrated into portable devices.

Transmitter design takes into account precise impedance matching between the amplifier stages and the antenna, frequency stability, attenuation interference and compliance with electromagnetic emission standards. Modern communication systems also use programmable transmitters, which allow dynamic change of operating parameters and adaptation to changing propagation conditions and network demand.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO