+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Ferroelectron emission is a physical phenomenon involving the release of electrons from the surface of a solid, usually a metal or Semiconductors, when exposed to high temperature. The process occurs when the thermal energy supplied to the material is sufficient to overcome a potential barrier called the exit work, allowing the electrons to leave the surface and pass into a vacuum or other medium.
The mechanism of thermoelectron emission is explained by the Fermi-Dirac model, according to which electrons in a metal are distributed according to a temperature-dependent energy distribution. An increase in temperature causes a certain number of electrons to gain energy greater than the value of the work of exit and can leave the material. A quantitative description of this phenomenon is given by the Richard-Dushman equation, which defines the current density of emission as a function of temperature and exit work.
This phenomenon is of key importance in vacuum and tube electronics. In electron tubes, such as Diodes, triodes or tetrodes, the cathode is heated to temperatures in the order of a few hundred to a few thousand kelvin (K), allowing a continuous flow of electrons to the anode. Thermionic emission is also used in electron guns, electron microscopy, cathode ray tubes and in thermionic energy converters, where it converts heat directly into electricity.
The efficiency of thermionic emission depends on the type of cathode material, its operating temperature, surface condition and vacuum conditions. In order to lower the required temperature, coatings with low work output, such as barium, strontium or lanthanum oxide compounds, are used. Modern designs also use semiconductor materials and nanostructures that allow emission control at lower energies.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.